I've been wrestling with stability issues as I am trying to reuse portions of the iMX6 Platform SDK in my boot loader. What I've found is that the memory map setup and the way stack is initialized, its possible that the stack pointer will not be double-word aligned. Apparently it is important to start off with this double-word alignment, because I've found that when I build my boot loader and the "top_of_stack" location is NOT double-word aligned (divisible by 8), then my system doesn't boot; however, if I adjust the memory map to force that to a double-word aligned address it does boot.
While I don't fully understand the need for this double-word alignment, there is some information here...
http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.faqs/ka4127.html
Anyway, the easy fix for this is to simply force this alignment in the linker file...
.stacks (NOLOAD) :
{
. = ALIGN (8); <<<<<< Add this line
__stacks_start = .;
. += 48K;
__stacks_end = .;
top_of_stacks = .;
} > DDR
This apparently is not a problem for folks using the SDK (perhaps something else in the build is forcing this alignment that I'm not aware of), so I'd like to get feedback on this post to see if folks agree or disagree with this suggested change.
解決済! 解決策の投稿を見る。
Right!
The quick fix is to do the ALIGN(8) that I show at the top.
The better fix is to apply the BIC instruction to all assignments of SP in that startup.S code...
@ set stacks for all other modes
msr CPSR_c, #MODE_FIQ | I_BIT | F_BIT
bic r0, r0, #15
mov sp, r0
sub r0, r0, r1
msr CPSR_c, #MODE_IRQ | I_BIT | F_BIT
bic r0, r0, #15
mov sp, r0
sub r0, r0, r1
msr CPSR_c, #MODE_ABT | I_BIT | F_BIT
bic r0, r0, #15
mov sp, r0
sub r0, r0, r1
msr CPSR_c, #MODE_UND | I_BIT | F_BIT
bic r0, r0, #15
mov sp, r0
sub r0, r0, r1
msr CPSR_c, #MODE_SYS | I_BIT | F_BIT
bic r0, r0, #15
mov sp, r0
sub r0, r0, r1
@ Set SVC mode stack with interrupts disabled
msr CPSR_c, #MODE_SVC | I_BIT | F_BIT
bic r0, r0, #15
mov sp, r0
sub r0, r0, r1
Found the below code in sdk/core/src/startup.S which should take care of this:
| /* | |||
| * fill the stacks with a pattern | |||
| * the stack must be 8 byte aligned | |||
| */ | |||
| ldr | r1,=__stacks_start | @ stack region start address | |
| ldr | r2,=top_of_stacks | @ stack region end address | |
| bic | r2,r2,#0x7 | @ round length down to nearest 8 byte alignment | |
| ldr | r3,=.Ldeadfeed | @ get fill pattern address | |
| ldr | r3,[r3] | @ read fill pattern into r3 | |
| mov | r4,r3 | @ copy fill pattern to r4 | |
| 1: cmp | r1,r2 | @ the fill loop | |
| stmltia r1!,{r3-r4} | |||
| blt | 1b |
Best regards,
-Mahesh
This does initialize the stack (which is good), but the important thing here is that the stack pointer itself be initialized with a value that is aligned. So I think my original post (showing the ALIGN(8) in the loader file) actually solved the problem for me. Actually, in my boot monitor code, I use the BIC instruction to adjust what ultimately is used as the stack pointer...
ldr r0, = (MonStack + MONSTACKSIZE - 4)
bic r0, r0, #15
mov sp, r0
Doing it this way (in code, rather than depending on an aligned tag) eliminates the need to care where the stack memory is. If you disagree, please let me know. I've had this fix in place for weeks now and it has been working just fine.
Looks like the SDK misses aligning the address written to sp.
Best regards,
-Mahesh
Right!
The quick fix is to do the ALIGN(8) that I show at the top.
The better fix is to apply the BIC instruction to all assignments of SP in that startup.S code...
@ set stacks for all other modes
msr CPSR_c, #MODE_FIQ | I_BIT | F_BIT
bic r0, r0, #15
mov sp, r0
sub r0, r0, r1
msr CPSR_c, #MODE_IRQ | I_BIT | F_BIT
bic r0, r0, #15
mov sp, r0
sub r0, r0, r1
msr CPSR_c, #MODE_ABT | I_BIT | F_BIT
bic r0, r0, #15
mov sp, r0
sub r0, r0, r1
msr CPSR_c, #MODE_UND | I_BIT | F_BIT
bic r0, r0, #15
mov sp, r0
sub r0, r0, r1
msr CPSR_c, #MODE_SYS | I_BIT | F_BIT
bic r0, r0, #15
mov sp, r0
sub r0, r0, r1
@ Set SVC mode stack with interrupts disabled
msr CPSR_c, #MODE_SVC | I_BIT | F_BIT
bic r0, r0, #15
mov sp, r0
sub r0, r0, r1
What is the file name to be edited?
Under the sdk directory:
apps/common/basic_sdk_app.ld.S