Porting WIFI SoftAP in Android 6.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting WIFI SoftAP in Android 6.0

Jump to solution
5,120 Views
petertseng
Contributor IV

Hi i.MX Community,

I try to porting WIFI modules BCM43241 to our i.MX6 custom board.

I can normally use WIFI to connect to the Internet.

But the following error occurs when I start SoftAp.

01-01 00:01:07.071: D/WifiHW_BCMDHD(1059): is_wifi_driver_loaded

01-01 00:01:07.071: W/WifiHW_BCMDHD(1059): Could not get driver status property!

01-01 00:01:07.136: D/WifiHW_BCMDHD(1059): insmod /system/lib/modules/bcmdhd.ko

01-01 00:01:07.810: D/Tethering(1059): sendTetherStateChangedBroadcast 0, 0, 0

01-01 00:01:07.810: D/Tethering(1059): InitialState.processMessage what=4

01-01 00:01:07.813: D/Tethering(1059): sendTetherStateChangedBroadcast 0, 0, 0

01-01 00:01:07.815: D/WifiHW_BCMDHD(1059): Wi-Fi interface property: wlan0

01-01 00:01:07.815: D/WifiHW_BCMDHD(1059): Check Wi-Fi interface ready!

01-01 00:01:07.817: D/WifiHW_BCMDHD(231): WIFI_GET_FW_PATH_AP=1

01-01 00:01:07.817: D/SoftapController(231): Softap fwReload - Ok

01-01 00:01:07.832: D/wifi(1059): Can not initialize the vendor function pointer table

01-01 00:01:07.832: E/WifiNative-HAL(1059): Could not start hal

01-01 00:01:07.832: E/WifiStateMachine(1059): Failed to start HAL

01-01 00:01:07.882: D/WifiHW_BCMDHD(231): ensure_entropy_file_exists

01-01 00:01:07.884: D/SoftapController(231): SoftAP started successfully

01-01 00:01:07.884: D/WifiHW_BCMDHD(1910): ensure_entropy_file_exists

01-01 00:01:07.884: E/SoftapController(1910): no specific driver vendor

01-01 00:01:07.884: E/SoftapController(1910): execl failed (Cannot assign requested address)

01-01 00:01:07.884: E/SoftapController(1910): SoftAP failed to start

01-01 00:01:07.886: E/WifiStateMachine(1059): Exception in softap start java.lang.IllegalStateException: command '26 softap startap' failed with '402 26 SoftAP command has failed'

01-01 00:01:07.887: E/SoftapController(1910): SoftAP is not running

01-01 00:01:07.888: D/WifiHW_BCMDHD(1910): WIFI_GET_FW_PATH_STA=0

01-01 00:01:07.888: D/SoftapController(1910): Softap fwReload - Ok

01-01 00:01:07.933: D/WifiHW_BCMDHD(1910): ensure_entropy_file_exists

01-01 00:01:07.935: D/SoftapController(1910): SoftAP started successfully

01-01 00:01:07.935: D/WifiHW_BCMDHD(1911): ensure_entropy_file_exists

01-01 00:01:07.935: E/SoftapController(1911): no specific driver vendor

01-01 00:01:07.935: E/SoftapController(1911): execl failed (Cannot assign requested address)

01-01 00:01:07.935: E/SoftapController(1911): SoftAP failed to start

01-01 00:01:07.937: E/WifiStateMachine(1059): Exception in softap re-start java.lang.IllegalStateException: command '30 softap startap' failed with '402 30 SoftAP command has failed'

01-01 00:01:07.939: E/WifiController(1059): WifiControllerSoftAP start failed

01-01 00:01:08.139: D/WifiHW_BCMDHD(1059): Unload driver module "bcmdhd"!

01-01 00:01:08.536: D/WifiHW_BCMDHD(1059): is_wifi_driver_loaded

01-01 00:01:08.536: D/WifiHW_BCMDHD(1059): wlan.driver.status=ok

01-01 00:01:08.537: W/WifiHW_BCMDHD(1059): The [bcmdhd] module not already exists!

01-01 00:01:25.797: I/MediaFocusControl(1059):  AudioFocus  abandonAudioFocus() from android.media.AudioManager@7a54129com.android.music.MediaPlaybackService$3@9ed6cae

01-01 00:01:25.825: I/ActivityManager(1059): Start proc 1912:com.android.musicfx/u0a12 for broadcast com.android.musicfx/.ControlPanelReceiver

01-01 00:01:25.915: W/System(1912): ClassLoader referenced unknown path: /system/priv-app/MusicFX/lib/arm

01-01 00:01:25.918: V/MusicFXControlPanelReceiver(1912): onReceive

01-01 00:01:25.918: V/MusicFXControlPanelReceiver(1912): Action: android.media.action.CLOSE_AUDIO_EFFECT_CONTROL_SESSION

01-01 00:01:25.918: V/MusicFXControlPanelReceiver(1912): Package name: com.android.music

01-01 00:01:25.918: V/MusicFXControlPanelReceiver(1912): Audio session: 9

01-01 00:01:25.919: V/MusicFXControlPanelEffect(1912): closeSession(android.app.ReceiverRestrictedContext@aec18d6, com.android.music, 9)

Hope for your help!

Regards,

0 Kudos
Reply
1 Solution
3,492 Views
petertseng
Contributor IV

Yes, I sure.

I found this patch will cause the 'hostapd' service could not start.

0001-ENGR00256988-wifi-load-diff-exec-in-start-softap.patch

Some people come across the same problem?

View solution in original post

0 Kudos
Reply
4 Replies
3,492 Views
SergioSolis
NXP Employee
NXP Employee

Can you erase or rename the following directory?:

"/data/misc/wifi"

and then try it again?

0 Kudos
Reply
3,492 Views
petertseng
Contributor IV

I try to delete the "/data/misc/wifi" directory and then reboot to startup SoftAP.

But the result is still the same.

0 Kudos
Reply
3,492 Views
SergioSolis
NXP Employee
NXP Employee

Did you make sure the directory was deleted after rebooting?, are you using a GA bsp or a user debug?

0 Kudos
Reply
3,493 Views
petertseng
Contributor IV

Yes, I sure.

I found this patch will cause the 'hostapd' service could not start.

0001-ENGR00256988-wifi-load-diff-exec-in-start-softap.patch

Some people come across the same problem?

0 Kudos
Reply