Porting LCD driver to uboot on imx8ulp

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Porting LCD driver to uboot on imx8ulp

2,103 次查看
wangrucheng
Contributor I

LCD parameters

static const struct display_timing default_timing = {
    .pixelclock.typ     = 27000000,
    .hactive.typ        = 480,
    .hfront_porch.typ   = 20,
    .hback_porch.typ    = 35,
    .hsync_len.typ      = 4,

    .vactive.typ        = 800,
    .vfront_porch.typ   = 10,
    .vback_porch.typ    = 20,
    .vsync_len.typ      = 4,
};
controller:st7701s
mipi lane:2
format: RGB888
mode:MIPI_DSI_MODE_VIDEO | MIPI_DSI_MODE_LPM | MIPI_DSI_MODE_VIDEO_BURST
    plat->lanes = priv->lanes;
    plat->format = MIPI_DSI_FMT_RGB888;
    plat->mode_flags = MIPI_DSI_MODE_VIDEO | MIPI_DSI_MODE_LPM | MIPI_DSI_MODE_VIDEO_BURST;
 
The same logic can run normally in the kernel, but it does not run properly in the uboot stage.

Can you give me some advice?

Thanks

 

0 项奖励
回复
5 回复数

2,077 次查看
brian14
NXP TechSupport
NXP TechSupport

Hi @wangrucheng

Thank you for contacting NXP Support.

This problem could be caused due to a difference in device tree used in both stages, U-boot and Kernel.
Please confirm that you are using the same device tree.

Have a great day!

0 项奖励
回复

2,015 次查看
wangrucheng
Contributor I

Hi @brian14

Have you ever checked this issue? I am currently stuck here and the deadline is very close.

Thanks!

0 项奖励
回复

2,073 次查看
wangrucheng
Contributor I

I am sure there is nothing wrong with the device tree I am using, because hx8394f panel can display the NXP log during the uboot startup phase.but my panel can't.

I uploaded device tree and panel code. 

0 项奖励
回复

2,003 次查看
brian14
NXP TechSupport
NXP TechSupport

Hi @wangrucheng

Could you please clarify your last reply?
In your first question you are saying that the problem is on uboot stage. However, in your last reply you are saying that your panel is working on uboot stage.

Also, I can't see your device tree or panel code. Could you please reupload your files?

Have a great day!

0 项奖励
回复

1,971 次查看
wangrucheng
Contributor I

I used a screen with ST7701S as the controller. Currently, the kernel can display the image normally, but when I porting it to uboot, I found that the NXP logo could not be displayed normally.

What I can confirm is that there is no problem with the device tree and there is no problem with the screen initialization code.

The attachment contains uboot kernel code and panel spec.

0 项奖励
回复