Please fix meta-imx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,484件の閲覧回数
mprt42
Contributor III

Hi,

I'm trying to build a yocto linux using your latest manifest:

repo init -u https://github.com/nxp-imx/imx-manifest.git -b imx-linux-scarthgap -m imx-6.6.52-2.2.0.xml

I get 7 errors for do_fetch (one is from meta-freescale, 6 from meta-imx):

Summary: 7 tasks failed:
/yocto/sources/meta-imx/meta-imx-bsp/recipes-graphics/imx-gpu-viv/imx-gpu-viv_6.4.11.p2.10-aarch32.bb:do_fetch
/yocto/sources/meta-imx/meta-imx-bsp/recipes-multimedia/imx-parser/imx-parser_4.9.2.bb:do_fetch
/yocto/sources/meta-freescale/recipes-bsp/imx-lib/imx-lib_git.bb:do_fetch
/yocto/sources/meta-imx/meta-imx-bsp/recipes-bsp/firmware-imx/firmware-imx_8.26.bb:do_fetch
/yocto/sources/meta-imx/meta-imx-bsp/recipes-graphics/imx-g2d/imx-gpu-g2d_6.4.11.p2.10.bb:do_fetch
/yocto/sources/meta-imx/meta-imx-bsp/recipes-connectivity/nxp-wlan-sdk/nxp-wlan-sdk_git.bb:do_fetch
/yocto/sources/meta-imx/meta-imx-bsp/recipes-kernel/kernel-modules/kernel-module-nxp-wlan_git.bb:do_fetch

Here are some stripped-down logs:

 

ERROR: imx-gpu-viv-1_6.4.11.p2.10-aarch32-r0 do_fetch: Fetcher failure: wget -t 2 -T 30 -O /mnt/d/yocto/downloads/imx-gpu-viv-6.4.11.p2.10-aarch32-accdd64.bin.tmp -P /mnt/d/yocto/downloads 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-viv-6.4.11.p2.10-aarch32-accdd64.bin' --progress=dot -v failed with exit code 8, see logfile for output
ERROR: imx-gpu-viv-1_6.4.11.p2.10-aarch32-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-viv-6.4.11.p2.10-aarch32-accdd64.bin;fsl-eula=true')

ERROR: imx-parser-4.9.2-r0 do_fetch: wget -t 2 -T 30 -O /mnt/d/yocto/downloads/imx-parser-4.9.2-828fcb7.bin.tmp -P /mnt/d/yocto/downloads 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-parser-4.9.2-828fcb7.bin' --progress=dot -v failed with exit code 8, see logfile for output
ERROR: imx-parser-4.9.2-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-parser-4.9.2-828fcb7.bin;fsl-eula=true')

ERROR: imx-lib-1_5.9+-r0 do_fetch: Fetcher failure: Unable to find revision 8f124c3914d82019849fb697baeb730e4cb1b547 in branch master even from upstream
ERROR: imx-lib-1_5.9+-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'git://github.com/nxp-imx/imx-lib.git;protocol=https;branch=master')

ERROR: firmware-imx-1_8.26-r0 do_fetch: Fetcher failure: wget -t 2 -T 30 -O /mnt/d/yocto/downloads/firmware-imx-8.26-d4c33ab.bin.tmp -P /mnt/d/yocto/downloads 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//firmware-imx-8.26-d4c33ab.bin' --progress=dot -v failed with exit code 8, see logfile for output
ERROR: firmware-imx-1_8.26-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//firmware-imx-8.26-d4c33ab.bin;fsl-eula=true')

ERROR: imx-gpu-g2d-6.4.11.p2.10-r0 do_fetch: Fetcher failure: wget -t 2 -T 30 -O /mnt/d/yocto/downloads/imx-gpu-g2d-6.4.11.p2.10-arm-accdd64.bin.tmp -P /mnt/d/yocto/downloads 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-g2d-6.4.11.p2.10-arm-accdd64.bin' --progress=dot -v failed with exit code 8, see logfile for output
ERROR: imx-gpu-g2d-6.4.11.p2.10-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-g2d-6.4.11.p2.10-arm-accdd64.bin;name=arm;fsl-eula=true')

ERROR: nxp-wlan-sdk-git-r0 do_fetch: Fetcher failure: Unable to find revision 5ad19e194f49ed9447bee7864eb562618ccaf9b1 in branch master even from upstream
ERROR: nxp-wlan-sdk-git-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'git://github.com/nxp-imx/mwifiex.git;protocol=https;branch=master')

ERROR: kernel-module-nxp-wlan-git-r0 do_fetch: Fetcher failure: Unable to find revision 5ad19e194f49ed9447bee7864eb562618ccaf9b1 in branch master even from upstream
ERROR: kernel-module-nxp-wlan-git-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'git://github.com/nxp-imx/mwifiex.git;protocol=https;branch=master')

 


thanks


 

0 件の賞賛
返信
1 解決策
1,455件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

HI @mprt42!
Thank you for contacting NXP Support!

The BSP version 6.1.52 is not officially launched yet.

We will Launch this version soon.

 

You can consult the latest release version in our web page.

 

Best Regards!

Chavira

元の投稿で解決策を見る

1 返信
1,456件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

HI @mprt42!
Thank you for contacting NXP Support!

The BSP version 6.1.52 is not officially launched yet.

We will Launch this version soon.

 

You can consult the latest release version in our web page.

 

Best Regards!

Chavira