Please check the power & por for iMX6D&Q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Please check the power & por for iMX6D&Q

跳至解决方案
1,404 次查看
chilwonna
Contributor II

Hi, All

I designed my board for iMX6D&Q.

Could you review the power&POR of my board.

Thanks.

标签 (2)
标记 (2)
0 项奖励
回复
1 解答
1,154 次查看
Yongxin
NXP Employee
NXP Employee

Hi chilwonna,

There are two comments of the design,

1. If the design is for i.MX6D/Q, the VDDARMxx_xx connection should follow Section 4.2 in AN4397.

<http://cache.freescale.com/files/32bit/doc/app_note/AN4397.pdf>

2. The power supply for U1052 VSNVS is not found, it is recommended to connect to VDDHIGH_IN.

Best Regards,

Yongxin

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,155 次查看
Yongxin
NXP Employee
NXP Employee

Hi chilwonna,

There are two comments of the design,

1. If the design is for i.MX6D/Q, the VDDARMxx_xx connection should follow Section 4.2 in AN4397.

<http://cache.freescale.com/files/32bit/doc/app_note/AN4397.pdf>

2. The power supply for U1052 VSNVS is not found, it is recommended to connect to VDDHIGH_IN.

Best Regards,

Yongxin

0 项奖励
回复
1,154 次查看
chilwonna
Contributor II

Hi, Yongxin Huang.

Thanks your reply.

1. I know that this design was optimized for iMX6Q.

    But I don't care power consumtion in my board.

    In this schematic, do not iMX6D work?

2. Thanks. I will fix.

Thanks. 

0 项奖励
回复
1,154 次查看
Yongxin
NXP Employee
NXP Employee

Hi chilwonna,

The power supply for i.MX6D and i.MX6Q in VDDARMxx_xx is different, if i.MX6D is used with i.MX6Q VDDARMxx_xx design, an extra leakage current on the chip and extra chip heating may occur. Unfortunately we don't perform such test so no data available for the replacement.

Best Regards,

Yongxin

0 项奖励
回复