Please check the power & por for iMX6D&Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Please check the power & por for iMX6D&Q

Jump to solution
1,143 Views
chilwonna
Contributor II

Hi, All

I designed my board for iMX6D&Q.

Could you review the power&POR of my board.

Thanks.

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
893 Views
Yongxin
NXP Employee
NXP Employee

Hi chilwonna,

There are two comments of the design,

1. If the design is for i.MX6D/Q, the VDDARMxx_xx connection should follow Section 4.2 in AN4397.

<http://cache.freescale.com/files/32bit/doc/app_note/AN4397.pdf>

2. The power supply for U1052 VSNVS is not found, it is recommended to connect to VDDHIGH_IN.

Best Regards,

Yongxin

View solution in original post

0 Kudos
Reply
3 Replies
894 Views
Yongxin
NXP Employee
NXP Employee

Hi chilwonna,

There are two comments of the design,

1. If the design is for i.MX6D/Q, the VDDARMxx_xx connection should follow Section 4.2 in AN4397.

<http://cache.freescale.com/files/32bit/doc/app_note/AN4397.pdf>

2. The power supply for U1052 VSNVS is not found, it is recommended to connect to VDDHIGH_IN.

Best Regards,

Yongxin

0 Kudos
Reply
893 Views
chilwonna
Contributor II

Hi, Yongxin Huang.

Thanks your reply.

1. I know that this design was optimized for iMX6Q.

    But I don't care power consumtion in my board.

    In this schematic, do not iMX6D work?

2. Thanks. I will fix.

Thanks. 

0 Kudos
Reply
893 Views
Yongxin
NXP Employee
NXP Employee

Hi chilwonna,

The power supply for i.MX6D and i.MX6Q in VDDARMxx_xx is different, if i.MX6D is used with i.MX6Q VDDARMxx_xx design, an extra leakage current on the chip and extra chip heating may occur. Unfortunately we don't perform such test so no data available for the replacement.

Best Regards,

Yongxin

0 Kudos
Reply