Pin reference on imx6slevk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pin reference on imx6slevk

ソリューションへジャンプ
2,421件の閲覧回数
carlosgallegos
Contributor III

Hi everybody,

I've been searching for a while and cannot seem to find a pin reference or a cross-reference between the pin names that appear in the schematics for the imx6slevk and the pin names that has to be used for editing the dts file. If anyone can provide me some help with this issue I will be more than thankful.

Greetings.

ラベル(4)
タグ(5)
1 解決策
2,125件の閲覧回数
carlosgallegos
Contributor III

Hi Luis,

Yeah that link help me in a way, but I've found what I was looking for, or at least something helpful. With the schematics and this header file linux/imx6sl-pinfunc.h at master · torvalds/linux · GitHub I can now define any pin I want.

Regards,

José Carlos

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,124件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hi Jose Carlos,

This link could help you

http://www.kosagi.com/w/index.php?title=Definitive_GPIO_guide

Regards,

Luis

2,126件の閲覧回数
carlosgallegos
Contributor III

Hi Luis,

Yeah that link help me in a way, but I've found what I was looking for, or at least something helpful. With the schematics and this header file linux/imx6sl-pinfunc.h at master · torvalds/linux · GitHub I can now define any pin I want.

Regards,

José Carlos

0 件の賞賛
返信