Pin reference on imx6slevk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pin reference on imx6slevk

Jump to solution
2,417 Views
carlosgallegos
Contributor III

Hi everybody,

I've been searching for a while and cannot seem to find a pin reference or a cross-reference between the pin names that appear in the schematics for the imx6slevk and the pin names that has to be used for editing the dts file. If anyone can provide me some help with this issue I will be more than thankful.

Greetings.

Labels (4)
1 Solution
2,121 Views
carlosgallegos
Contributor III

Hi Luis,

Yeah that link help me in a way, but I've found what I was looking for, or at least something helpful. With the schematics and this header file linux/imx6sl-pinfunc.h at master · torvalds/linux · GitHub I can now define any pin I want.

Regards,

José Carlos

View solution in original post

0 Kudos
Reply
2 Replies
2,120 Views
LuisCasado
NXP Employee
NXP Employee

Hi Jose Carlos,

This link could help you

http://www.kosagi.com/w/index.php?title=Definitive_GPIO_guide

Regards,

Luis

2,122 Views
carlosgallegos
Contributor III

Hi Luis,

Yeah that link help me in a way, but I've found what I was looking for, or at least something helpful. With the schematics and this header file linux/imx6sl-pinfunc.h at master · torvalds/linux · GitHub I can now define any pin I want.

Regards,

José Carlos

0 Kudos
Reply