Pin mapping of GPIO7 is missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pin mapping of GPIO7 is missing

Jump to solution
1,950 Views
K_Steinhammer
Contributor III

Where can I find the pin mapping of GPIO7 for the iMX8QM.

GPIO7 is defined in the address map, but there is no pin mapping defined in the Chip IO section of the SOCs reference manual.

As I am running out of GPIO pins, this information would be highly appreciated...

 

Thanks

0 Kudos
Reply
1 Solution
1,934 Views
jimmychan
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
2 Replies
1,930 Views
K_Steinhammer
Contributor III

OK, thanks for the confirmation...

0 Kudos
Reply
1,935 Views
jimmychan
NXP TechSupport
NXP TechSupport

Yes, there is no GPIO7.

This is the pads of i.mx8qm defined in the bsp.

https://source.codeaurora.org/external/imx/linux-imx/tree/include/dt-bindings/pinctrl/pads-imx8qm.h?...

 

0 Kudos
Reply