Pin mapping of GPIO7 is missing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Pin mapping of GPIO7 is missing

跳至解决方案
1,681 次查看
K_Steinhammer
Contributor III

Where can I find the pin mapping of GPIO7 for the iMX8QM.

GPIO7 is defined in the address map, but there is no pin mapping defined in the Chip IO section of the SOCs reference manual.

As I am running out of GPIO pins, this information would be highly appreciated...

 

Thanks

0 项奖励
回复
1 解答
1,665 次查看
jimmychan
NXP TechSupport
NXP TechSupport
0 项奖励
回复
2 回复数
1,661 次查看
K_Steinhammer
Contributor III

OK, thanks for the confirmation...

0 项奖励
回复
1,666 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Yes, there is no GPIO7.

This is the pads of i.mx8qm defined in the bsp.

https://source.codeaurora.org/external/imx/linux-imx/tree/include/dt-bindings/pinctrl/pads-imx8qm.h?...

 

0 项奖励
回复