Pin Multiplexing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pin Multiplexing

2,261件の閲覧回数
abhi_kr
Contributor I

I am using MCIMX7D5EVM10SD for a project and want to utilize the EIM interface to communicate to FPGA,Also I want to use the two Ethernet port available.I am planning to use the First 8 AD lines from the EIM so that i can allocate the other pins for the two Ethernet. Is this possible.

0 件の賞賛
返信
3 返答(返信)

2,231件の閲覧回数
abhi_kr
Contributor I

Hi @riteshmpatel ,

I am using the Config tool only for the pin multiplexing .My concern is for example if we are having 20 pins for the EIM and i am using only 10 and the rest i had assigned for the two Ethernet related pins by the help of the tool,tool is supporting this.My question is if i am driving the Ethernet pins which was taken from the EIM pins will it affect the EIM operation,whether the opposite also will happen?

0 件の賞賛
返信

2,221件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @abhi_kr,

Since the tool allows the pin muxing, it won't affect each other's functionality.

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信

2,251件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @abhi_kr,

I hope you are doing well.

One can download the Config Tools for i.MX Applications Processors and perform the pin muxing and check if it can suffice one's requirement of the interfaces desired to be used.

I hope it helps!

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信