Pin Multiplexing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pin Multiplexing

2,259 Views
abhi_kr
Contributor I

I am using MCIMX7D5EVM10SD for a project and want to utilize the EIM interface to communicate to FPGA,Also I want to use the two Ethernet port available.I am planning to use the First 8 AD lines from the EIM so that i can allocate the other pins for the two Ethernet. Is this possible.

0 Kudos
Reply
3 Replies

2,229 Views
abhi_kr
Contributor I

Hi @riteshmpatel ,

I am using the Config tool only for the pin multiplexing .My concern is for example if we are having 20 pins for the EIM and i am using only 10 and the rest i had assigned for the two Ethernet related pins by the help of the tool,tool is supporting this.My question is if i am driving the Ethernet pins which was taken from the EIM pins will it affect the EIM operation,whether the opposite also will happen?

0 Kudos
Reply

2,219 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @abhi_kr,

Since the tool allows the pin muxing, it won't affect each other's functionality.

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply

2,249 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @abhi_kr,

I hope you are doing well.

One can download the Config Tools for i.MX Applications Processors and perform the pin muxing and check if it can suffice one's requirement of the interfaces desired to be used.

I hope it helps!

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply