Phylink support in ethernet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Phylink support in ethernet

2,416 Views
kunal_003
Contributor III

Hi all,

We are planning to use the SFP module for ethernet interface in i.MX6SX chipset. In order to use SFP phylink framework should be used. STMAC supports phylink, however, the FEC MAC driver is using the phylib framework. We are following this link for adding the phylink support. My concern is does NXP support or have integrated the phylink framework in FEC? If not, are there any plans to integrate in future release?

We are using kernel version L4.14. It has phylink and SFP support.

Any pointer or help on this is appreciated.

 

Regards,

Kunal

0 Kudos
Reply
3 Replies

2,410 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

2,404 Views
kunal_003
Contributor III

Hi @igorpadykov ,

 

Thank you for quick response.

 

It seems the link that you shared is a reference and the enetc is PCIe ethernet controller, is this correct understanding?

I was looking for phylink support in "fec_main.c" (FEC MAC driver), which is using phylib framework. Does ethernet driver supports phylink and can we use it directly?

 

Regards,

Kunal

0 Kudos
Reply

2,396 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kunal

 

sorry, I think you are right:  "fec_main.c" has not phylink support.

For plans to integrate it in future releases suggest to contact local marketing office.

 

Best regards
igor

0 Kudos
Reply