Phone app is not visible on menu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Phone app is not visible on menu

3,641 Views
oslreddy
Contributor II

Hi all,

I am working on i.MX6q sabereSD board with Android 4.2

When I build and flash my image I am not able to find Phone app on menu

Can anybody tell me is there any change I need to make for phone app to be visible

I am able to find com.android.phone in pm list packages output but in menu no icon related to phone app is present

Regards

O S L Reddy

5 Replies

2,543 Views
chenguoyin
NXP Employee
NXP Employee

It is controled by the feature you declared in your board. You can have it as below:

imx6/sabresd_6dq.mk

@@ -29,7 +29,6 @@ PRODUCT_COPY_FILES += \

        frameworks/native/data/etc/android.hardware.wifi.direct.xml:system/etc/permissions/android.hardware.wifi.direct.xml \

        frameworks/native/data/etc/android.hardware.sensor.light.xml:system/etc/permissions/android.hardware.sensor.light.xml \

        frameworks/native/data/etc/android.hardware.sensor.accelerometer.xml:system/etc/permissions/android.hardware.sensor.accelerometer.xml \

+       frameworks/native/data/etc/android.hardware.telephony.gsm.xml:system/etc/permissions/android.hardware.telephony.gsm.xml \

        frameworks/native/data/etc/android.hardware.faketouch.xml:system/etc/permissions/android.hardware.faketouch.xml \

        frameworks/native/data/etc/android.hardware.sensor.barometer.xml:system/etc/permissions/android.hardware.sensor.barometer.xml \

        frameworks/native/data/etc/android.hardware.camera.front.xml:system/etc/permissions/android.hardware.camera.front.xml \

+++ b/sabresd_6dq/required_hardware.xml

@@ -25,8 +25,6 @@

  -->

     <feature name="android.hardware.location" />

     <feature name="android.hardware.location.network" />

+   <feature name="android.hardware.telephony" />

+   <feature name="android.hardware.telephony.gsm" />

     <feature name="android.hardware.wifi" />

     <feature name="android.hardware.touchscreen" />

     <feature name="android.hardware.touchscreen.multitouch" />

0 Kudos
Reply

2,543 Views
max_tsai
NXP Employee
NXP Employee

Android 4.2.2 needs extra setting as below.

--

device/fsl/sabresd_6dq/overlay/frameworks/base/core/res/res/values/config.xml

@@ -183,7 +183,7 @@

     <bool name="config_showNavigationBar">true</bool>

     <!-- This device is not "voice capable"; it's data-only. -->

-    <bool name="config_voice_capable">false</bool>

+    <bool name="config_voice_capable">true</bool>

     <!-- Max space (in MB) allocated to DownloadManager to store the downloaded files

          if they are to be stored in DownloadManager's data dir,

2,543 Views
xianyoju
Contributor II

Android 4.2.2_1.0.0-ga


I also have this problem!!

the Camera app not visible on menu too!

0 Kudos
Reply

2,542 Views
oslreddy
Contributor II

I Tried to install one third party phone app

In that When I am trying to call it is telling

Tellephony feature is not available in this device

Can anybody tell me how to enable telephony feature in sabereSD JB 4.2

0 Kudos
Reply

2,543 Views
xianyoju
Contributor II

who can solve the problem?

0 Kudos
Reply