Performance problems after changing the linux kernel from version 3.10.53 to 4.1.15

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Performance problems after changing the linux kernel from version 3.10.53 to 4.1.15

1,457 次查看
trsystems
Contributor II

We are facing a general performance problem with kernel 4.1.15. In general the applications seem to be about 25% slower than under Kernel 3.10.53. We are using the same UBoot for both kernels with the same DDR-RAM configuration.

Has anyone had the same problem?

Any ideas?

标签 (2)
0 项奖励
回复
1 回复

1,356 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Oliver

please check as possible reason

Cortex-A9 ARM Errata 845369 

Also one can try with nxp official bsps from link below, they use kernel 3.10.53 with

uboot v2014.04 and kernel 4.1.15 with uboot v2015.04

i.MX 6 Series Software and Development Tool|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复