Performance SDMA transfer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Performance SDMA transfer

Jump to solution
1,965 Views
larstraeger
Contributor II

Hello community,

i'd like to know which type of " uart 2 external memory" sdma transfer is faster. Should i use a shared Uart connect to SDMA via SPBA or is the access over the Functional Unit Peripheral/Burst Units for "normal" Uarts faster.

thanks and regards

Lars

Labels (3)
0 Kudos
Reply
1 Solution
1,624 Views
JerryFan
NXP Employee
NXP Employee

SPBA bus is preferred, since it is dedicated to SDMA, and thus bus swithch, bus competition(specailly for IP bus which connected with a lot of peripheral), if Functional Unit Peripheral used,  can be avoided.  

View solution in original post

0 Kudos
Reply
1 Reply
1,625 Views
JerryFan
NXP Employee
NXP Employee

SPBA bus is preferred, since it is dedicated to SDMA, and thus bus swithch, bus competition(specailly for IP bus which connected with a lot of peripheral), if Functional Unit Peripheral used,  can be avoided.  

0 Kudos
Reply