Partial Image Authentication in HAB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Partial Image Authentication in HAB

1,390 Views
norratheprattan
Contributor I

I'm not sure if my previous question has been noticed since I put it in a comment. So I'll put it here instead.

Based on my understanding of HAB and HAB uImage Layout, uImage is authenticated as a whole by u-boot. and it seems to be the case for example API provided in a document.

Is there a code (and/or is it possible at all in HAB) for authenticating only a partial uImage since some parts of our image (at least at the end) should support a code update.

Thanks,

Labels (3)
0 Kudos
Reply
1 Reply

1,315 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Basically boot ROM HAB API is used just to check an area in memory,

so, if customer's uImage can be split into two parts - it is possible to sign

only one of them (based on uImage memory layout).  

Have a great day,

Yuri

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

0 Kudos
Reply