Parallel camera Device tree entries.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Parallel camera Device tree entries.

2,637 次查看
subbaraopnv
Contributor I

Hi,

In iMX7, We are going to interface a parallel camera. What are the device tree entries are required for a parallel camera?

Thanks,
Subbarao.

标签 (2)
0 项奖励
回复
2 回复数

2,301 次查看
subbaraopnv
Contributor I

Hi Igor,

Thanks for your reply.

Input available to CSI interface is RGB24, i,e 24 bits / Clk. 

In iMX7 Reference manual, section "13.3 CMOS Sensor Interaface" it is mentioned that it supports RGB24. But when I captured a frame from the CSI interface it is not as expected. 

What is the CSI register configuration required to enable RGB24 capture.

Thanks,
Subbarao.

0 项奖励
回复

2,300 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Subbaro

I am not aware of parallel camera dts for i.MX7, but as it has the same CSI module

as i.MX6UL, SL one can look at its dts:

linux/arch/arm/boot/dts/imx6ul-14x14-evk-csi.dts

imx6ul-14x14-evk-csi.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

imx6sl-evk-csi.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

About preview function in i.MX6SL. 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复