Parallel RGB lcd display support on iMX6Q Android

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Parallel RGB lcd display support on iMX6Q Android

1,950件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi All,
I have parallel RGB lcd display connect with imx6q Android 7.1.2 platform. I have set bootargs also 'video=mxcfb0:dev=lcd,EDT-VGA,if=RGB24' with this parameter. But I'm not getting anything on display.

Can you help on this to bring up lcd.?

Regards,
Aravinth

ラベル(5)
0 件の賞賛
返信
1 返信

1,510件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Aravinth

NXP i.MX6Q reference boards do not have parallel lcd,

for parallel lcd configuration one can look at boundary devices android releases for
okaya display used with BD-SL-i.MX6, Nitrogen6X, Nitrogen6_MAX, and Nit6X:
imx6qdl-nitrogen6x.dtsi
linux-imx6/imx6qdl-nitrogen6x.dtsi at boundary-imx_4.1.15_1.0.0_ga · boundarydevices/linux-imx6 · Gi... 
Android Nougat 7.1.1 release for i.MX6 boards - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信