GS2101M wifi module driver for i.MX6 linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GS2101M wifi module driver for i.MX6 linux

1,977 次查看
minkyungseo
Contributor I

Hello!

I have to porting the GS2101M wifi module to some custom board. GS2101M module is product of ‘Telit’(the former name is ‘Gainspan’) and it is using GS2000 SoC.

My platform is linux(kernel version 3.10), so I’m searching the linux driver of GS2010M module.

And I found two links when I searching the linux driver.

Please, look at this.

http://www.gainspan.com/newsroom/article_02242015_linux_drivers

https://community.nxp.com/docs/DOC-331802

After found them, I requested supporting the linux driver to Telit agency. But they said, they are not support linux driver because their linux engineers were resign after merger of Gainspan and Telit.

That time, I heard freescale developed GS2000 linux driver with Gainspan.

So I requested to freescale agency. But they not answerd.

I searched the driver in freescale linux and android bsps, but I can’t found it.

Last, I’m writing this Question letter.

Can anyone advice me about the GS2101M linux driver?

 

Thank you.

0 项奖励
回复
1 回复

1,574 次查看
igorpadykov
NXP Employee
NXP Employee

Hi MinKyung

for available nxp drivers one can look at linux documentation

https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser...

and also  post this to meta-fsl-arm mailing list, so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复