Parallel RGB lcd display support on iMX6Q Android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Parallel RGB lcd display support on iMX6Q Android

2,021 Views
aravinthkumarja
Senior Contributor II

Hi All,
I have parallel RGB lcd display connect with imx6q Android 7.1.2 platform. I have set bootargs also 'video=mxcfb0:dev=lcd,EDT-VGA,if=RGB24' with this parameter. But I'm not getting anything on display.

Can you help on this to bring up lcd.?

Regards,
Aravinth

0 Kudos
Reply
1 Reply

1,581 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aravinth

NXP i.MX6Q reference boards do not have parallel lcd,

for parallel lcd configuration one can look at boundary devices android releases for
okaya display used with BD-SL-i.MX6, Nitrogen6X, Nitrogen6_MAX, and Nit6X:
imx6qdl-nitrogen6x.dtsi
linux-imx6/imx6qdl-nitrogen6x.dtsi at boundary-imx_4.1.15_1.0.0_ga · boundarydevices/linux-imx6 · Gi... 
Android Nougat 7.1.1 release for i.MX6 boards - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply