Panel can't display correct Android screen

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Panel can't display correct Android screen

1,372件の閲覧回数
bensonhuang
Contributor II

Hi,

We are using i.MX8M for our development platform.

Panel is 800x480 resolution (7 inch).

We use Yocto Linux and Android to test if the panel can display the screen.

For Yocto Linux (fsl-yocto-L4.9.51_mx8mq-ga), the panel can display correct screen of x-wayland.

For Android (imx-o8.0.0_1.3.0_8mq-prc), we can't show the correct screen.

The attached files are the frame buffer shown on Vyson and the screen shown on the panel.

Could you please help to give us some advice how to solve the issue?

Thanks.

S__27508753.jpg

S__27508752.jpg

ラベル(4)
0 件の賞賛
返信
1 返信

1,252件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Can you please tell me the display that you are using? 

Best Regards,

Diego

0 件の賞賛
返信