Packet loss RGMII

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Packet loss RGMII

2,509 Views
himanshugusain
Contributor III

Hi

We have connected RGMII back to back between IMX and ZYNQ

Also we have taken care of PHY simulation in our driver.

The problem we are facing currently is while pinging "IMX <-> ZYNQ" with payload

we are seeing the packet loss.

This issue (PacketLoss) was not observed in freescale provided 3.0.35 kernel ,but is currenly observed

in 3.10.53 kernel

I have seen additional things like flow control has been added in 3.10.53 kernel

also there are few changes w.r.t  tx/rx flow .

Could that be resulting in packetloss issue

Labels (3)
0 Kudos
Reply
2 Replies

2,049 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Himanshu,

Yes, this changes could be the result of packetloss, since as you may already known the i.MX6 FEC Controller, has an errata. Please see more details in the following link:

i.MX6 Ethernet limitations

0 Kudos
Reply

2,049 Views
himanshugusain
Contributor III

Hi James

I am unable to access above link

Regards

Himanshu

0 Kudos
Reply