PWM1 submodule2 doesn't output pwm signal iMXRT1050

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PWM1 submodule2 doesn't output pwm signal iMXRT1050

747件の閲覧回数
pamela_mz
Contributor I

Hi,
I am trying to configure GPIO_SD_B0_05 as PWM1 output, I do not need any interrupts, the pwm frequency should be 80Hz or 1kHz with a duty cycle of 80%.

The configuration that I have are shown below.

PIN config

IOMUXC_SetPinMux(IOMUXC_GPIO_SD_B0_05_FLEXPWM1_PWMB02, 0U);

MODE config

IOMUXC_SetPinConfig(IOMUXC_GPIO_SD_B0_05_FLEXPWM1_PWMB02, 0x10B0U);

PWM Config

pwm_config_t PWM1_UIOreset1_M1_SM2_config =
{
//submodule 2 from PWM1 channel B
.enableDebugMode = true,
.enableWait = true,
.reloadSelect = kPWM_LocalReload,
.faultFilterCount = 0,
.faultFilterPeriod = 0,
.clockSource = kPWM_BusClock,
.prescale = kPWM_Prescale_Divide_128,
.initializationControl = kPWM_Initialize_LocalSync,
.forceTrigger = kPWM_Force_LocalSync,
.reloadFrequency = kPWM_LoadEveryOportunity,
.reloadLogic = kPWM_ReloadImmediate,
.pairOperation = kPWM_Independent,
};

Signal Parameters

pwm_signal_param_t PWM1_UIOreset1_M1_SM2_pwm_function_config =
{
.pwmChannel = kPWM_PwmB,
.dutyCyclePercent = pwm_dutycycle,
.level = kPWM_HighTrue,
.deadtimeValue = 0U,
};

status_t PWM_setup_stat = 0;

PWM_setup_stat = PWM_SetupPwm(PWM1, kPWM_Module_2, &PWM1_UIOreset1_M1_SM2_pwm_function_config, 1U, kPWM_EdgeAligned, 80, 3000000U);

PWM_SetPwmLdok(PWM1, kPWM_Control_Module_2, true);

status_t init_pwm = PWM_Init(PWM1, kPWM_Module_2, &PWM1_UIOreset1_M1_SM2_config);

PWM_StartTimer(PWM1, kPWM_Control_Module_2);

 

I have debugged and verify the registers values, but still can't get to output the pwm signal from the pin.

Has anyone an idea or is there a configuration that I'm missing?

Thanks!

0 件の賞賛
返信
1 返信

726件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi @pamela_mz

Thank you so much for your interest in our products and for using our community.

Please check SDK example evkbimxrt1050_pwm, in Config Tools add pin J2 (GPIO_SD_B0_05) as shown below:

nxf86756_0-1666296203140.jpeg

Run the example and on pin 2 of the SD Card (SD1_D3) of the MIMXRT1050-EVK you will see the PWM signal you need.

nxf86756_1-1666296223254.jpeg

Hope it helps you.

Have a nice day!

0 件の賞賛
返信