PWM API / PWM Library for IMX Linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PWM API / PWM Library for IMX Linux

跳至解决方案
5,261 次查看
rvalvekar
Contributor III

Hello Community,

I am searching for libraries which can be used for PWM Operations especially with the stepper motors. I would like to interface with IMX Processors. 

I have searched on this community and on third party vendors, but i could not find any libraries which are focused on PWM. 

Do I need any kind of Hardware with the stepper motor for implementing motors ? For example motor control chipset ?

I would like some support from Community on this topic.

Thanks for Support and Help.

R.

0 项奖励
回复
1 解答
4,902 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Rohan,

Linux BSP for i.MX processors include a basic PWM library (mainly oriented for LCD backlight control). Therefore, it is not intended to work with more real-time implementations like motor control and may not fit your timing requirements. Please refer to chapter 2.7 “Pulse-Width Modulator (PWM)” section of “i.MX Reference Manual” document (attached) for additional details.

In case of using a heterogeneous i.MX processor like the i.MX6SX, i.MX7 or i.MX8, you could use the included M4 core to control real-time applications, like motor control.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
4,903 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Rohan,

Linux BSP for i.MX processors include a basic PWM library (mainly oriented for LCD backlight control). Therefore, it is not intended to work with more real-time implementations like motor control and may not fit your timing requirements. Please refer to chapter 2.7 “Pulse-Width Modulator (PWM)” section of “i.MX Reference Manual” document (attached) for additional details.

In case of using a heterogeneous i.MX processor like the i.MX6SX, i.MX7 or i.MX8, you could use the included M4 core to control real-time applications, like motor control.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 项奖励
回复
4,903 次查看
rvalvekar
Contributor III

Hello Carlos,

Thank you for the information.

0 项奖励
回复