PN7150 tag detection time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7150 tag detection time

1,584件の閲覧回数
divyeshmarne0
Contributor III

Hi NXP Team,

We are using PN7150 NFC controller with custom board IMX8MM. Which supports Android 11 code base.

So our requirement specify that, PN7150 RFID reader shall respond in less than 500ms to then scanning tag.

divyeshmarne0_0-1655881323634.png

Need your inputs on following points-

1. To support this, Do we need to make any software changes?

2. If RFID could support this, Please provide reference for this. ( I cant find any reference in datasheet).

Attaching working logs and porting guide. 

Thanks

Divyesh

ラベル(1)
0 件の賞賛
返信
1 返信

1,582件の閲覧回数
divyeshmarne0
Contributor III

This RFID should respond in less than 500ms when we place tag near to the RFID.

0 件の賞賛
返信