PMU registers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMU registers

Jump to solution
1,778 Views
takashitakahash
Contributor III

Hi community.

I have question For the following PMU registers.

· PMU_REG1P1 (Addr: 20C_8110)

· PMU_REG3P0 (Addr: 20C_8120)

· PMU_REG2P5 (Addr: 20C_8130)

The above are three of the PMU register, There are description of "i.MX 6Solo / 6DualLite Applications Processor Reference Manual" of Although the Rev0 ,but  it has been removed from Rev1 in description and MemoryMap.

question.

1, Could you tell us about deleted reason.

2, Is it no probrem to change these registers from BSP in our products.

Labels (4)
0 Kudos
Reply
1 Solution
1,664 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

1. these descriptions will be back again in rev.2 of Reference Manual

2. no problem

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,665 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

1. these descriptions will be back again in rev.2 of Reference Manual

2. no problem

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply