PMIC support in linux kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PMIC support in linux kernel

2,414件の閲覧回数
sagarkadam
Contributor I

Hello,

We are planning to use MMFP0100A family PMIC device into our Custom SoC (ARM) based platform,which will have linux-4.4.16 running onto it.

We have not encountered any device driver for this device. Could you please let us know if device driver for this device is present into Linux kernel available on the git.

Any reference links would be helpful.

Thanks & BR,

Sagar 

ラベル(1)
0 件の賞賛
返信
1 返信

1,742件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Sagar Kadam,

The driver is available on the i.MX6 BSPs, however, please note that the latest BSP release supports kernel 4.1.15.  Perhaps you would like to take a look at the Community BSP, which is part of the Yocto Project and Open Sourced (link below):

http://freescale.github.io/

Regards,

0 件の賞賛
返信