PMIC support in linux kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMIC support in linux kernel

2,397 Views
sagarkadam
Contributor I

Hello,

We are planning to use MMFP0100A family PMIC device into our Custom SoC (ARM) based platform,which will have linux-4.4.16 running onto it.

We have not encountered any device driver for this device. Could you please let us know if device driver for this device is present into Linux kernel available on the git.

Any reference links would be helpful.

Thanks & BR,

Sagar 

Labels (1)
0 Kudos
Reply
1 Reply

1,725 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Sagar Kadam,

The driver is available on the i.MX6 BSPs, however, please note that the latest BSP release supports kernel 4.1.15.  Perhaps you would like to take a look at the Community BSP, which is part of the Yocto Project and Open Sourced (link below):

http://freescale.github.io/

Regards,

0 Kudos
Reply