PMIC selection for i.MX6ULL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PMIC selection for i.MX6ULL

1,170件の閲覧回数
ben_jones
Contributor I

Hi,

I am working on a new design using the i.MX6ULL and intending to use the PF3001 for the PMIC as I don't need the additional features in the PF3000.

Can someone please confirm that the PF3001 is compatible with the i.MX6ULL? The data sheet for the PF3001 only confirms that the i.MX6UL is supported, and doesn't mention the i.MX6ULL.

Thanks,

Ben

ラベル(3)
0 件の賞賛
返信
1 返信

1,088件の閲覧回数
nxf54947
NXP Employee
NXP Employee

Hello Ben,

You can see the i.MX 6ULL as a derivation from i.MX 6UL. I would suggest you to check the migration guide from i.MX 6UL to i.MX 6ULL:

Migrating from i.MX 6UL to i.MX 6ULL

You can use the PF3001 datasheet to help you selecting a PMIC for your processor (Table 1. Orderable part variations):

PF3001 datasheet

I hope the information was helpful!

Regards,

0 件の賞賛
返信