PMIC RTC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PMIC RTC

1,771件の閲覧回数
srirammadhu
Contributor I

HI... I'am using iMX53 processor that runs wince7.

I have issues in using PMIC(DA9052) RTC instead of iMX53 RTC.

So can anybody tell me how to use the PMIC RTC?? and any other supported links or docs??

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

1,562件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Unfortunately we do not have a reference design that uses the DA9052 RTC to feed the i.MX53. (Freescale’s i.MX53QSB does use a DA9053 but does not make use of the RTC and rather has a 32kHz crystal connected to the i.MX53 oscillator).

However, Freescale’s i.MX53 Start-R board uses a MC34708 PMIC to generate the RTC and then it feeds it to the i.MX53 processor. I would suggest downloading this schematic and using it as reference.

0 件の賞賛
返信