PMIC: PCA9450

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PMIC: PCA9450

3,134 次查看
saidjazouly
Contributor III

Hello,

We designed a customer's solution based on i.MX8M processor and using the PCA9450 as the PMIC.

Our questions is:

Are the PCA9450's registers volatile after power cycling the board or do they keep their last modified values?

 

Thanks for your help!

0 项奖励
回复
4 回复数

3,128 次查看
saidjazouly
Contributor III

Thanks for your help Igor!

0 项奖励
回复

3,130 次查看
igorpadykov
NXP Employee
NXP Employee

Hi saidjazouly

 

not sorry, in general case registers value are not preserved. Datasheet can be found on link

https://www.nxp.com/products/power-management/pmics-and-sbcs/pmics/power-manage-ic-pmic-for-i-mx-8m-...

 

Best regards
igor

0 项奖励
回复

3,115 次查看
saidjazouly
Contributor III

Hi Igor,

our customer is wondering if there is a way to preserve the register values through power-cycles. The reason being at board power-up, the new PMIC settings should take effect even before the i.MX8 has a chance to access in read/write the PMIC registers.

Is there anyway to preserve those registers new values and to only change them when the i.MX decides to do so?

 

Thanks for your help.

0 项奖励
回复

3,108 次查看
igorpadykov
NXP Employee
NXP Employee

Hi saidjazouly

 

> way to preserve the register values through power-cycles. The reason being at board power-up,
>the new PMIC settings should take effect even before the i.MX8 has a chance to access in read/write
>the PMIC registers.

 

default register values are hardcoded so I am afraid it is not feasible, sorry.

 

Best regards
igor

0 项奖励
回复