PHY Addressing using 2 PHYs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PHY Addressing using 2 PHYs

ソリューションへジャンプ
2,309件の閲覧回数
jautry
Contributor IV

I am building a design around an MIMXRT 1062 using both MACs with 2 external PHYs.  Since each MAC module has separate MDIO and MDC signals, can I have the PHY hardwired addresses the same eg 1 or do they still have to be different.

タグ(1)
0 件の賞賛
返信
1 解決策
2,292件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply and clarfication.
1) Can these addresses by hardwired the same if using the separate MDIO and MDC signals.
-- Yes.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,302件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Can I have the PHY hardwired addresses the same eg 1 or do they still have to be different.
-- According to your statement, you want to use the same MDC and MDIO to access the same registers in both of PHY chips, in my opinion, it's possible to make it, however, I'd highly don't recommend the developer to do that.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,298件の閲覧回数
jautry
Contributor IV

I think the question was misunderstood.  I am using the separate MDIO and MDC signals provided by the 1062.  The 2 phys have their own hardwired addresses.  Can these addresses by hardwired the same if using the separate MDIO and MDC signals.

タグ(1)
0 件の賞賛
返信
2,293件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply and clarfication.
1) Can these addresses by hardwired the same if using the separate MDIO and MDC signals.
-- Yes.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信