PHP support for IMX8MQ yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PHP support for IMX8MQ yocto

3,415 Views
nagendrasarma
Contributor III

Hello NXP

we are using imx8m evk + yocto latest distribution  4.14.98 

we would like to add PHP and  light-httpd support 

could you please help us in adding above packages 

regards

Nagendra  

Tags (1)
0 Kudos
Reply
6 Replies

3,231 Views
nagendrasarma
Contributor III

you mean to say add apache2 support and rebuild the qt5 image ?

any link to achieve the same ? 

my target is to run web server on imx8mq platform 

0 Kudos
Reply

3,231 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

You are right the image is just supported in MX8, but you have to build the package image with the apache on it.

Regards

0 Kudos
Reply

3,231 Views
nagendrasarma
Contributor III

i am trying to add apache to imx8 + 'fsl-image-qt5-validation-imx' and getting following error 

ERROR: Required build target 'fsl-image-qt5-validation-imx' has no buildable providers.

Missing or unbuildable dependency chain was: ['fsl-image-qt5-validation-imx', 'apache2']

is imx8mq + fqt5 image support web server ? 

if yes which web server is better and how to add to yocto ?

0 Kudos
Reply

3,231 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

the fsl.image-qt5-validation-imx is only supported by MX6UL, MX6ULL and MX7D.

Regards

0 Kudos
Reply

3,231 Views
nagendrasarma
Contributor III

Hello  Bio,

please find attached image for reference, according to nxp-yocto-imx documentation rev: L4.14.98_2.0.0_ga 4/2019

fsl-image-qt5-validation-imx is NOT supported on imx6ul, imx6uLL imx7dual

so, please help me in making yocto project with php.apache2, and lhttpd on imx8mq evk ?

New Bitmap Image.bmp

0 Kudos
Reply

3,231 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello nagendra,

I’ve seen this question also in external forums, I hope that they can provide some guidance as there is no documentation for running php on the i.MX.

 

I’ve found the following thread in an external forum, perhaps it can help. Although I’m guessing maybe you already found it while searching on the web.

Install PHP via Yocto - Toradex Community 

Regards

0 Kudos
Reply