PF8100 conversion efficiency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PF8100 conversion efficiency

跳至解决方案
484 次查看
kpoyuan
Contributor I

HI NXP Teams

How should the conversion efficiency of the PF8100 Type 1 and Type 2 buck regulators be evaluated? Currently, when the load is below 10mA, the conversion efficiency is less than 50%. Is this normal, or are there any other suggested modifications?

0 项奖励
回复
1 解答
436 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

This can be verified in registers SWx_RUN_MODE and SWx_STBY_MODE, by default is configured with autoskip mode.

Best regards.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
440 次查看
kpoyuan
Contributor I

HI

The PF8100 also supports the autoskip mode, which seems to allow automatic adjustment between PWM and PFM based on load conditions. How can I determine when the IC will switch between these modes?

0 项奖励
回复
437 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

This can be verified in registers SWx_RUN_MODE and SWx_STBY_MODE, by default is configured with autoskip mode.

Best regards.

0 项奖励
回复
470 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

There is no available benchmarks for PF8100, the efficiency should be measured using the relation between input and output power.

To operate under the PMIC specifications please use the datasheet as reference for your design (component values, connections, layout, etc.).

Best regards.

0 项奖励
回复