PF3001 regulators

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF3001 regulators

4,332 Views
riteshpatel
Contributor II


Hi,

I am using PF3001 PMIC in my design to power iMX6UL processor.

PF3001 is available with pre-programmed OTP configuration to support iMX6UL. Programming option is 7 (i.MX 6UL with DDR3L) and part # is MC32PF3001A7EP. As PF3001 Datasheet page # 3.

As per power startup sequence shown for programming option A7 on PF3001 datasheet page #29. Sequences of VLDO2 and 3 are OFF.

So can we leave floating VLDO2IN, VLDO2 & VLDO3 pins?? Here floating means leaving floating without decoupling capacitors.

Thanks,

Ritesh.

0 Kudos
Reply
9 Replies

3,528 Views
dhvanil_patel1
Senior Contributor I

Hi Luis,

Thanks for quick response.

I think this patch is related PF300 PMIC.  I need patch for PF30001 PMIC.

Can you please share what changes should I have to change in order to use PF300 u-boot driver for PF30001 PMIC.

-

Dhvanil

0 Kudos
Reply

3,528 Views
dhvanil_patel1
Senior Contributor I

Hi Luis Casado,

Is PF30001 PMIC patch available for u-boot ? If yes , can you please share PF30001 PMIC patch for u-boot ?

-

Dhvanil

0 Kudos
Reply

3,528 Views
LuisCasado
NXP Employee
NXP Employee
0 Kudos
Reply

3,528 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ritesh

one can follow AN4717 Schematic Guidelines for the MMPF0100

recommendations for unused ldos

http://cache.freescale.com/files/analog/doc/app_note/AN4717.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,528 Views
riteshpatel
Contributor II

Thank you igor for your quick response.

I am using PF3001 in my design. Suggested AN4717 sch guideline is for

PF0100. So can i use this recommendations for PF3001 too.??

0 Kudos
Reply

3,528 Views
igorpadykov
NXP Employee
NXP Employee

yes, this is the same family of pmics using similar technology.

0 Kudos
Reply

3,528 Views
riteshpatel
Contributor II

Hi Igor,

Thank you for your extended support.

We are using PF3001 PMIC in our project.

Is it possible to use PF3000 PMIC drivers on PM3001 PMIC?

If yes, What changes are required?

0 Kudos
Reply

3,528 Views
LuisCasado
NXP Employee
NXP Employee

Hi,

1.      You have patch for PF3001:

2.      http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/commit/drivers/regulator/pfuze100-regula... d=19708058f049be9a5dcc81943d1b9a14080367e8

1.     

Luis.

3.     

0 Kudos
Reply