imx6s H.264 Encoding

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,663件の閲覧回数
505053487
Contributor I

         I refer to the VPU Example Application and wirte an application program to encode streams  from camera captured data. VPU example application is located under Yocto Project build tmp work tree in imx-test/*/test/mxc_vpu_test.

          Then I get a video file named ”my.h264". But when I play the video file .  Video quality is not good .

`YEDLVSX}XA2`ZJ%RAB}`{U.jpg

     What does this problem produce?  I think my parameter setting is not good . But I donnot know how to modify. Help,thank you. By the way,my English is really terrible.

ラベル(3)
0 件の賞賛
返信
1 解決策
2,419件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

could you share more detailed information? what parameter do you use??

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,420件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

could you share more detailed information? what parameter do you use??

0 件の賞賛
返信
2,419件の閲覧回数
505053487
Contributor I

Too many lines of codes.  The source camera data is YUV420p format in memory.

For example:

  /* Fill up parameters for encoding */

  encop.bitstreamFormat     = STD_AVC;

  encop.mapType                =  0;          //where 0 = Linear frame map; 1 = Frame tiled map; 2 = Field tiled map

  encop.linear2TiledEnable  = 0;                 

  encop.frameRateInfo = 20;

  encop.bitRate = 0;      

  encop.gopSize = 1;       // where 0 = only first picture is I, 1 = all I pictures, 2 = IPIP, 3 = IPPIPP, and so on.

  encop.slicemode.sliceMode = 0;   /* 0: 1 slice per picture; 1: Multiple slices per picture */

  encop.slicemode.sliceSizeMode = 0; /* 0: silceSize defined by bits; 1: sliceSize defined by MB number*/

  encop.slicemode.sliceSize = 4000;  /

    encop.IntraCostWeight = 0;

    encop.MEUseZeroPmv  = 0;

    /* (3: 16x16, 2:32x16, 1:64x32, 0:128x64, H.263(Short Header : always 3) */

    encop.MESearchRange = 3;

    encop.userGamma = (Uint32)(0.75*32768);         /*  (0*32768 <= gamma <= 1*32768) */

    encop.RcIntervalMode= 1;        /* 0:normal, 1:frame_level, 2:slice_level, 3: user defined Mb_level */

    //encop.RcIntervalMode= 0;

    encop.MbInterval = 0;

    encop.avcIntra16x16OnlyModeEnable = 0;

    encop.ringBufferEnable = enc->ringBufferEnable;   

    encop.dynamicAllocEnable = 0;

    encop.chromaInterleave = 0;                        // CbCr interleaved , default is interleave(1)

0 件の賞賛
返信