PF3000 : current limit value

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PF3000 : current limit value

732 次查看
koichisakagami
Contributor II

Dear community,
We have been developing our product with PF3000.
I am checking a PF3000 data sheet.


I found the different parameters between tables.

For example,
    ISW2LIM value is 2.5A (Typ)( SW2ILIM = 0) at Table 9. Static electrical characteristics.
    However, ISW2LIM value is 2.75A (Typ)( SW2ILIM = 0)  at Table 162. SW2CONF field descriptions.

[Question]
Which is the correct value , SWxxCONF field descriptions table or Static electrical characteristics table ?

       Best Regards,
       Koichi Sakagami

标签 (1)
0 项奖励
回复
1 回复

643 次查看
art
NXP Employee
NXP Employee

The ISW2LIM parameter means the current value that triggers on the current limiter circuit. As it can be seen in the Table 9, this value is very average and can vary from approx. 1.6A to approx 3.4A. So, both 2.5A and 2.75A values can be treated as the "typical" ones.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复