PF1550+i.MX6ULL recommended connection for INT2P7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF1550+i.MX6ULL recommended connection for INT2P7

872 Views
yuji_matsunami
Contributor II

Hi,
Regarding application note(AN12055)
The application note(AN12055) has been updated Rev2.0 and the connections of 38pin(INT2P7) have changed when not used.
What is the reason for the change?
also, what will happen if 38pin(INT2P7) is floating ?


AN12055 Rev2.0    Page.2
38pin INT2P7 Recommended connection when not used : Bypass with 2.2uF capacitor to ground

AN12055 Rev1.0     Page.3
38pin INT2P7 Recommended connection when not used : Leave floating

0 Kudos
Reply
1 Reply

861 Views
jamesbone
NXP TechSupport
NXP TechSupport

The change it is only for a better termination of the PIN, for removing the power distortion and noise and protect the system/IC by providing pure DC supply.

 

0 Kudos
Reply