PF0200 interrupt handler in Yocto 3.10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF0200 interrupt handler in Yocto 3.10

869 Views
davesimonson
Contributor I

How do I use/handle the INTB interrupt from the PF0200 PMIC in Yocto 3.10?

Labels (4)
0 Kudos
Reply
1 Reply

784 Views
igorpadykov
NXP Employee
NXP Employee

Hi DAVE

INTB interrupt could be used as fault event, like pmic overheating or

overcurrent described in Table 100. Interrupt, Mask and Sense Bits

MMPF0200 Datasheet

http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0200.pdf

Seems currently this interrupt is not used in linux.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply