Dear all,
We design a board using i.MX6Quad and PF0100.
We look at datasheets of i.MX6Qual and PF0100.
However, we think that Currents of SW1A/B and SW1C of PF0100 are not enough.
How should we understand this in designing?
In the SBRE-SD board, these are connected as follows.
- PF0100 SW1A/B [2500mA] => i.MX6Q VDDCORE(VDD_ARM_IN+VDD_ARM23_IN) [Max 3730mA]
- PF0100 SW1C [2000mA] => i.MX6Q VDDSOC(VDD_SOC_IN) [Max 2370mA]
For i.MX6Quad

For PF0100

May I have advice?
Best Regards,
Yuuki