PF0100 Programming Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF0100 Programming Error

6,750 Views
legbam5
Contributor I

The verify after programming shows errors. 

legbam5_LEGNB0555_2019-07-15-000042.jpg

After repowering and verify "NO programming erros" appears.

I don't understand it.

The error code 0x05 in fuse bank 0xE3 is not descibed in AN4536.

Labels (1)
0 Kudos
Reply
1 Reply

6,667 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

 

Can you please check if the PMIC is already programmed before you try to program it, please?

 

You can do this by clicking on the “Blank Check” button.

 

If the PMIC is already programmed, it will not be possible to re-program it and this could be the cause of the programming errors you are seen.

0 Kudos
Reply