PF0100 OTP programming issue.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF0100 OTP programming issue.

ソリューションへジャンプ
3,912件の閲覧回数
tihomirpetrov
Contributor I

Last year i work on my own board with i.MX6, but i have some problems with PF0100NPEP.

In TBB mode everything is ok. I set desired output voltage, power sequencing and etc. Everything work fine.

After that i try to program OTP, but nothing can happen. Button "PROGRAM" on "KTPF0100GUI REV 3.0.0.20:" does not working.:smileyshocked:

I try to use "Read_Configuration.txt" script and got following:

Script has been loaded.

Date: 27.1.2014 г. Time: 21:17 ч.

Script File Used: Read_Configuration.txt

SW1AB OTP Vout = 0,3000 Volts

SW1AB OTP Sequence = 0

SW1AB OTP Config: A/B/C Single Phase, Freq = 1 MHz

SW1C OTP Vout = 0,3000 Volts

SW1C OTP Sequence = 0

SW1C OTP Config: Freq = 1 MHz

SW2 OTP Vout = 0,4000 Volts

SW2 OTP Sequence = 0

SW2 OTP Config: Freq = 1 MHz

SW3A OTP Vout = 0,4000 Volts

SW3A OTP Sequence = 0

SW3A OTP Config: A/B Single, Freq = 1 MHz

SW3B OTP Vout = 0,4000 Volts

SW3B OTP Sequence = 0

SW3B OTP Config: Freq = 1 MHz

SW4 OTP Vout = 0,4000 Volts

SW4 OTP Sequence = 0

SW4 OTP Config: Freq = 1 MHz, VTT = Off

SWBST OTP Vout = 5.000 Volts

SWBST OTP Sequence = 0

VGEN1 OTP Vout = 0,8 Volts

VGEN1 OTP Sequence = 0

VGEN2 OTP Vout = 0,8 Volts

VGEN2 OTP Sequence = 0

VGEN3 OTP Vout = 1,8 Volts

VGEN3 OTP Sequence = 0

VGEN4 OTP Vout = 1,8 Volts

VGEN4 OTP Sequence = 0

VGEN5 OTP Vout = 1,8 Volts

VGEN5 OTP Sequence = 0

VGEN6 OTP Vout = 1,8 Volts

VGEN6 OTP Sequence = 0

VREFDDR OTP Sequence = 0

VSNVS OTP Vout = 1,0000 Volts

OTP Sequencer CLK Speed = 0.5 msec

OTP DVS CLK Speed = 2.0 usec

OTP PWRON Mode = Level Sensitive

OTP PGOOD = Off

Script Run Complete


I try to install KITPFGUI, Rev. 4.0.0.12, but it does not find KITPFPGMEVME


what did i do wrong?


ラベル(2)
0 件の賞賛
返信
1 解決策
3,384件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Petrov,

Unfortunately we have seen an incompatibility between some KITPFPGMEVME HW with the new GUI revision 4.0.0.12 and unfortunately, the problem that you are seen looks like a problem with the GUI 3.0.0.20 which is no longer supported, so I would recommend you to use the newer version of the KITPFPGMEVME HW or us the instruction mentioned in the application note AN4536 (http://cache.freescale.com/files/analog/doc/app_note/AN4536.pdf) for the OTP programming.

Regards,

Jose

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,384件の閲覧回数
tihomirpetrov
Contributor I

So... I installed software on other PC, but same situation... :smileyangry:

Is there anyone help me to program OTP?

0 件の賞賛
返信
3,384件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Petrov,

First I would like to check in which revision of the GUI we need to concentrate in, only the KITPFPGMEVME Rev.B (Labeled with a "REV.B" Sticker) is compatible with the GUI 4.0.0.12 version. Can you please let me know if you have the REV B programmer, please?

Regards,

Jose Reyes

0 件の賞賛
返信
3,384件の閲覧回数
tihomirpetrov
Contributor I

Hello,

Thanks for your reply.

Yes KITPFGMEVME is Rev B. This is a sticker and packing list:  

IMAG1238_1.jpgIMAG1240_1.jpg

0 件の賞賛
返信
3,385件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Petrov,

Unfortunately we have seen an incompatibility between some KITPFPGMEVME HW with the new GUI revision 4.0.0.12 and unfortunately, the problem that you are seen looks like a problem with the GUI 3.0.0.20 which is no longer supported, so I would recommend you to use the newer version of the KITPFPGMEVME HW or us the instruction mentioned in the application note AN4536 (http://cache.freescale.com/files/analog/doc/app_note/AN4536.pdf) for the OTP programming.

Regards,

Jose

0 件の賞賛
返信
3,384件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

reyes,  Can you please  help?

0 件の賞賛
返信