PDM mic driver (non-Linux) for i.MX8M Mini

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PDM mic driver (non-Linux) for i.MX8M Mini

1,509件の閲覧回数
nxa14910
NXP Pro Support
NXP Pro Support

A customer would like to use the PDM mic interface on an i.MX8M Mini processor but they cannot use Linux. Therefore they are in need of a driver that is suitable for bare metal or to be used with an RTOS. Has such a driver been developed internally or are you aware of an open source solution that can be leveraged. 

This is fairly urgent so any input or guidance that can be provided is appreciated.

Thank you,

Doug Bruce

ラベル(1)
0 件の賞賛
返信
1 返信

1,460件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Doug 

one can check MCUXpresso SDK_EVK-MIMX8M Mini (*/driver_examples/pdm folder),

build it on

Welcome | MCUXpresso SDK Builder 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信