PDM MIC issues i.MX93

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PDM MIC issues i.MX93

2,176件の閲覧回数
mohamed_gaseen
Contributor IV

Hello,

I'm recently working on the PDM microphone enablement on the i.MX93 evaluation board. The issue is that the interrupt is not detected. The audio got captured but while playing the audio the sound didn't appear. I have attached the audio capturing log file below for your reference.

Microphone details:  Adafruit 4346 PDM Microphone Breakout with JST SH Connector

Below I have attached the interrupt log.

root@imx93EVK:~# cat /proc/interrupts | grep mic
116: 0 0 GICv3 234 Level micfil
117: 0 0 GICv3 233 Level micfil
118: 0 0 GICv3 232 Level micfil
119: 0 0 GICv3 231 Level micfil

Below is the command I've used for recording the audio.

arecord -f S32_LE -d 10 -r 48000 --device="hw:1,0" capture.wav -vvv

The PDM Mic /etc/asound.conf file configuration:

defaults.pcm.rate_converter "linear"

# spk represents the physical sink (playback)
pcm.spk
{
type plug
slave.pcm "hw:wm8962audio,0"
}

# mic represents the physical source (capture)
pcm.mic
{
type plug
slave.pcm "hw:micfilaudio,0"
}

Please support me to sort out this issue.

Thanks in Advance.

 

 

ラベル(1)
0 件の賞賛
返信
1 返信

2,139件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

do you mind checking the result with command "aplay -l"

0 件の賞賛
返信