PCN 201409001F01 -Clarification Required

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCN 201409001F01 -Clarification Required

2,015 Views
kasibalaji
Contributor I

Hi Team,

Greetings!!!

We have received the PCN document # 201409001F01 from NXP. In the PCN, the detailed change is mentioned as follows:

Wafer production for the display drivers PCF85176T (in TSSOP56) and PCF85162T (in TSSOP48) will move from TSMC to Vanguard (VIS). The semiconductor process will remain the same. Also the specification will be unchanged except some minor changes in current consumption.
We also change the wire bonding material from gold (Au) to copper (Cu). There will be no effect in form or function related to this change.

I just wanted to know the exact information about the current consumption change. Please let me know the exact change in current consumption of the part. Also i need the completed Qualification Report. Currently the report which i have, is not fully qualified one(attached the report fyr).

The part we are using in the design is : PCF85162T/1

Your earliest reply in this regard is highly appreciated.

Thanks,

Kasi

0 Kudos
Reply
1 Reply

1,867 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Kasi,

In this time, we encourage you to submit your question through a Case; please refer to the following Community document:

How to submit a new question for NXP Support

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply