PCM/I2S support on imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCM/I2S support on imx6q

1,321 Views
bikash
Contributor II

Hi,

On our custom board, we are going to use a codec which gives PCM output.

Please let us know in perspective of IMX6Q processor, how PCM differs from I2S.

At many places, it is mentioned that PCM is similar to I2S.

Could  we use the same "ssi interface" driver  for  both PCM & I2S.

Thanks,

Bikash

Labels (2)
0 Kudos
Reply
2 Replies

1,133 Views
sumit8915
Contributor III

Hi Bikas,

Have to come to any conclusion regarding this?

Thanks

Sumit

0 Kudos
Reply

1,133 Views
igorpadykov
NXP Employee
NXP Employee

Hi bikash

"PCM" word is too generic and vague to provide accurate answer,

some PCM formats may be supported, some not.

Suggest to check codec datasheet and compare with i.MX6 RM SSI chapter

to understand if it can be supported.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply