PCIe memory alignment and size

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCIe memory alignment and size

1,180 次查看
jimmykwon
Contributor I

we have 4 EP devices each have 8MB access requirement.

but i can read from manual "PCIe max memory alignment is 16MB for i.MX 6 quad."

Can i.MX 6 access 4 EP devices each have 8MB ?

In iATU, it can has 4 regions. then

first iATU set : 8MB  for first EP

second iATU set : 8MB for second EP

third iATU set : 8MB for third EP

fourth iATU set : 8MB for fourth EP

is it possible ?

0 项奖励
回复
1 回复

1,066 次查看
art
NXP Employee
NXP Employee

Q. Can i.MX 6 access 4 EP devices each have 8MB ?

A. Unfortunately, no. The total amount of memory for all endpoints is limited to 16MB.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复