PCIe link timeout issue on iMX6Q smart device board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCIe link timeout issue on iMX6Q smart device board

ソリューションへジャンプ
1,747件の閲覧回数
pingchuanma
Contributor I

Hi experts,

The SDK PCIe test fails on iMX6Q smart_device board. It shows:

Please make sure the mini pcie card inserted. Type"y" or "Y" to confirm.
Link timeout.
PCIE init failed.

Was the PCIe source code validated on iMX6Q smart device board? Thanks a lot.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,548件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi pingchuan,

SDK works well please refer to attached file (based on SDK).

You can try other card.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,549件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi pingchuan,

SDK works well please refer to attached file (based on SDK).

You can try other card.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,548件の閲覧回数
pingchuanma
Contributor I

The board is smart_device_rev_c

0 件の賞賛
返信