PCIe endpoint driver with DMA support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCIe endpoint driver with DMA support

2,279 次查看
shabbirlimdiwal
Contributor I

Hi,

Is i.mx6 quad validated with PCIe end point mode in Linux? Is DMA implementation already available for PCIe end point?

We have a high throughput requirement (output 720P30, YUV422) over PCIe. Will i.mx6 quad be sufficient enough to do so?

Thanks and Regards,

Shabbir

标记 (2)
0 项奖励
回复
1 回复

1,549 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Shabbir

yes it is validated

i.MX6Q PCIe EP/RC Validation System

please also check attached document sect.35.5 i.MX 6Quad SD PCIe RC/EP Validation System

included in L3.0.35_4.1.0_ER_SOURCE_BSP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复